AXIS#.IL.LIMITP

Description

This parameter sets the positive user limit clamp value of the torque-producing q-component current command (AXIS#.IL.CMD). The current command is additionally limited by the motor peak current setting (AXIS#.MOTOR.IPEAK ) and by the present value of the foldback I²t peak motor current protection.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write

Units

A

Range

0 A to drive peak current (IPEAK)

Default Value

Drive peak current (IPEAK)

Data Type

Float

See Also

AXIS#.IL.LIMITN

Stored in Non-Volatile Memory

Yes

Variants Supported

All variants are supported.

Industrial Ethernet Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

AXIS1.IL.LIMITP

500ah

04h

Signed32

-

1000:1

Read/Write

No

EtherNet/IP

ID

Instance

Attribute

Name

Data Type

Access

User Mappable

5814

1

5814 (0x16b6)

AXIS1.IL.LIMITP

Signed32

Read/Write

Yes

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS1.IL.LIMITP

5814

Float

Read/Write

-